USER.INT#
Description
Set of scratchpad variables users can use for read and write. Keywords can be selected as an Action Table source.
Examples
Usage
Code
Map to Modbus -->MODBUSModBus is a serial communications protocol and is now the most commonly available means of connecting industrial electronic devices. ModBus is often used to connect a supervisory computer with a remote terminal unit in supervisory control and data acquisition (SCADA) systems. Versions of the ModBus protocol exist for serial port and Ethernet (it is widely used with TCP/IP over Ethernet).MAP 40001 USER.INT2
Setup Action -->ACTION5.TASK 12 -->ACTION5.TASKID 1 -->ACTION5.SOURCE 23 -->ACTION5.SOURCEID 2 -->ACTION5.CONDITION 12 -->ACTION5.CONDITIONVALUE 20 -->ACTION5.ACTION 1
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-03-04-000 |
|
General Information
|
Type |
Read/Write |
| Units | N/A |
|
Range |
-32768 to 32767 |
| Default Value | 0 |
|
Data Type |
Integer |
| See Also | ACTION#.SOURCE 23 |
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
- | 4100h | 1-10 | INT | - | - | RW | False |